Hello,
I am using the two Buck -TI part TPS54560BQDDARQ1 for the DC-DC converter. One for the output 12VDC /5A and second is for 5VDC/5A.
My input is 9V-32VDC.
I have attached my schematic is below. when I am checking the output at no load condition then the Output voltage showing 12VDC and 5VDC. But when I am applying the load for it, then my output gets turn- off (no voltage at output). even i apply just 50mA load then it becomes no output. I didn't understand, why I am getting this issue. my schematic okay as per TI-recommended circuit. please give me any solution.