This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24030

Other Parts Discussed in Thread: BQ24030, TPS63020

Hi,

Please check with TI if I need the battery charging status:

-          Battery voltage level

-          Battery capacity level (value or percent)

Can this info imported from the charger IC?

 

At the BQR24030 CE pin should connect to both AC input and USB input (with shcotkey diodes) – or there is other option?

 

 

At the BQR24030 there are 2 pins STAT1 and STAT2 that gives the charging status (page 24 in the data sheet, table 2).

I do not see a status of regular charging.

If I need status of regular charging, and also status when charging goes to complete:

Let say led that blink fast when battery is almost empty and charging. As long as the battery advance in charging and capacity and voltage increasing the led blink slower and slower until its completely or on. Can I get this feature directly from the component?

If I connect those 2 pins directly to microprocessor input:

when its ON , the STAT pin is output=0 ?

When STAT pin is off , then what the MC pin will see? Do I need to tie the MC pin to Vcc?

 Regarding the BQ24030 if the following:

-          AC input 5V

-          USB input 5V

-          Single LI-IO battery (3.7-4.2 typical voltage)

What is the output voltage range at the out pins?

When VCC to charger is 5V, and the output connects to TPS63020DSJ, designed to Vout of 5V, will it affect on the output voltage, and how?

At TPS63020DSJ, when EN pin =0, then Vout is 0V?

Thanks,

Shlomi

 4010.POWER SUPPLY PAGE2.pdf