Will the TPSF12C3 AEF IC work at 400 Hz line frequency for aerospace applications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the TPSF12C3 AEF IC work at 400 Hz line frequency for aerospace applications?
Hi Vijay,
With sensing capacitors (CSEN1-4) of 680pFand TPSF12C3 internal components, the combination creates a high-pass filter that attenuates 50Hz/60Hz line frequency by ~100dB. At 400Hz of line frequency, the rejection is less and the IC will see around 50 times more of the 400Hz signal than the standard 50Hz/60Hz signal. The IC will work at 400Hz of line frequency but there may be some line frequency signal appearing on the output of the INJ pin.
Ben
Thanks, Ben, that clarifies things. However, even if some line frequency signal appears on the output of the INJ pin at 400 Hz, it should manifest as a differential mode noise signal, and that should not matter if I am trying to get rid of common mode. Is that correct? Should I simply reduce the Csns caps, and try with an eval board, or will the scheme just not work?
Hi Vijay,
The IC rejects DM noise and only focuses on CM noise. The 680pF sense caps creates an optimal high-pass filter response that rejects 50Hz/60Hz signals and would not recommend other values. You can order a single-phase EVM filter board to evaluate its performance.
Ben