I'm planning to use the LDO part LP5912-1.8DRVR to generate a 1.8V output using a 2.5V input. From the LP5912 datasheet, I'm able to confirm that we can generate 1.8V using a 2.5V input voltage (VIN = VOUT + 0.5V). However, even though the distributor's website shows that the part LP5912-1.8DRVR is for a 1.8V output, I couldn't find any datasheet or orderable part number information confirming that the LP5912-1.8DRVR can generate a 1.8V output. Could you please provide confirmation, as well as the datasheet or links confirming that the part LP5912-1.8DRVR can generate a 1.8V output? Thank you