Part Number: BQ24295
Other Parts Discussed in Thread: BQ25619
Our circuit uses BQ24295 with a wireless power receiver.
The wireless power receiver outputs ~5VDC.
The battery capacity is 320 mAh so theoretically the charging current should be limited to 160 mAh.
As there is no USB input, D+ and D- pins are left floating. Perhaps this is an issue afterthought.
We tried to set the limit and the charging current
- reg_write_byte(0x00, 0x5a);
- 1A (100)
- If we choose 500 mA (010), it doesn’t seem to charge
- ILIM is 1K
- reg_write_byte(0x02, 0x1C);
- Charge Current 448 mA
- The battery capacity is 320mA
Also we added a Schottky diode to prevent the current from flowing in the reverse direction.
The issue is that despite the sufficient charging current set up in the register and ILIM, the battery doesn't seem to get charged.
The wireless power should provide enough current at 5V, > 500 mA.
Is there some D+/D- detection we would need to disable since they are left floating?
Or how should we terminate them since there is no USB input.
The attached Powerpoint shows the circuits for BQ24295 and the wireless power receiver (STWLC68 from STMicro).
Regards,
Andrew