Looking at the Electrical characteristics table in the SLVSFT0A datasheet (revised December 2021), the VBIAS Shutdown Current is listed as typ. 0.1uA, max. 0.2uA @ -40 to 85*C and max. 0.27uA at -40 to 125*C for VBIAS=3.3V. Looking at the graph (figure 7-2), the Shutdown Current is between 3 and 6 uA for -40 to 85*C and around 9uA for 125*C. Is the graph incorrect?
Also the Quiescent Current graph (figure7-1) is inconsistent with the table. For TPS22992 it is listed as typ. 10uA, max. 15uA @ -40 to 85*C and max. 16uA at -40 to 125*C for VBIAS=3.3V. For the TPS22992S it is listed as typ. 26uA, max. 42uA @ -40 to 85*C and max. 45uA at -40 to 125*C for VBIAS=3.3V. The graph shows 25-27uA for 3.3VBIAS, could it be for the "S"?
These characteristics are very important to our design, so I would very much appreciate some clarification.
Thanks and regards,
Mari