This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206: Power on sequence

Part Number: TPS51206
Other Parts Discussed in Thread: TMDS64EVM, TPS51200

Hello team,

I am confused on power on sequence of this device.

On datasheet 7.3.6, it says "During power on, it is allowed to turn on VDD, S3 and S5 first, then turn on VLDOIN and VDDQSNS."
However, on Figure 23, it looks like VLDOIN and VDDQSNS is powered up before S5 and S3.

Which line should I power up first?

On the schematic of TMDS64EVM (PROC101D(004)), looks like S3 and S5 is powered up at the same timing. Also VDD and VLDOIN is powered up at the same time.

Is it okay to power up S3 & S5 and VDD & VLDOIN at the same timing?

What is the correct power up sequence for each power lines?

Best Regards,
Kei Kuwahara