Other Parts Discussed in Thread: BQ25185, BQ24040, BQ25180
Hi,
if you could suggest the Li-ion/PO single cell battery charges, with capacity of max current =1A, but settable to 500mA or less for USB based application
Input DC voltage 4.75V to 5.5V DC
should have good thermal handling, charge status indication
Regards,