Hello Ti Engineers,
I have a number of questions regarding the BQ24133 charging circuit
1. What is the minimum resistance that can be used for Rac? The value of Rac in the datasheet examples are 20mΩ. Since our system has a typical continuous current of 8A (Max). We were considering lowering the Rac to minimize the voltage drop across. Can we go with 10mΩ?
2. Does the BQ24133 have a Input In-Rush Current limit?, If we set IDPM to 8.5A. What would the scenario be if the charger is disabled and system has an inrush current >9A for a few seconds? How does the Charger Circuit behave? will it disable the ACFET and RBFET? If The BQ24133 does not have an in rush charge current protection. Do you have a recommended part for that?
3. What is the minimum input voltage for a 2S Application (max li-ion battery voltage of 8.42V)? Can 9V be used? Does it have a limitation for what fast charge current can be used?
Thanks,
Deniel