HI Ti team
Will the BQ25798 automatically stop charging after the BQ25798 is triggered to the fast charging timer? Or the MCU that controls the BQ25798 needs to send instructions to stop charging
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The BQ25798 should not need a MCU for charge termination.
Best Regards,
Christian.
* Created: Fri Apr 05 10:28:21 CST 2024 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * BQZ Container: Charger_2_00-bq25798.bqz * REG00 00 0E REG01 01 41A REG03 03 12C REG05 05 88 REG06 06 12C REG08 08 43 REG09 09 01 REG0A 0A A8 REG0B 0B DC REG0D 0D 03 REG0E 0E 38 REG0F 0F E2 REG10 10 50 REG11 11 78 REG12 12 08 REG13 13 21 REG14 14 86 REG15 15 AA REG16 16 C0 REG17 17 02 REG18 18 3B REG19 19 32 REG1B 1B 00 REG1C 1C 00 REG1D 1D 01 REG1E 1E 00 REG1F 1F 00 REG20 20 00 REG21 21 00 REG22 22 00 REG23 23 00 REG24 24 00 REG25 25 00 REG26 26 00 REG27 27 00 REG28 28 FF REG29 29 47 REG2A 2A 7F REG2B 2B 1F REG2C 2C 00 REG2D 2D 00 REG2E 2E A0 REG2F 2F 00 REG30 30 00 REG31 31 00 REG33 33 00 REG35 35 00 REG37 37 00 REG37 39 00 REG3B 3B 2454 REG3D 3D 247C REG3F 3F 24C REG41 41 38 REG43 43 CE3 REG45 45 CEA REG47 47 00 REG48 48 19
HI TI team
Attached is the register configuration file of my BQ25798 and the data of BQ25798 LOG. After charging for more than 15h, the charging does not stop, and the fast charge timmer does not work. Please help check why the fast charge timmer does not work
Hello,
Can you run a test by increasing termination current to 320mA, to see if this resolves the issue?
I think the low termination current might be the issue:
Best Regards,
Christian.