This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM62440-Q1: RFBT minimum value

Part Number: LM62440-Q1

Hi team,

Could you advise if there is a mandatory requirement for minimum RFBT value of LM62440-Q1?

it is described in the datasheet below, but I would like to use below 10kohm. 

"Usually RFBT is between 10 kΩ and 1 MΩ."

This device automatically select Fixed voltage or adjustable voltage at start up, so I concern if selecting <10kohm causes any issue selecting adjustable output at startup.

regards,

  • Hi Tsuji-san,

    This device does not automatically select between fixed output voltage or adjustable voltage at startup. The customer would need to order the correct OPN for a fixed 3.3V or 5V output option or an adjustable version. See below:

    I don't see a problem using resistors values lower than 10Kohms but I would advise to be careful with the power rating of the top resistor. Also, using smaller value feedback resistors will mean a higher value feed-forward capacitor, if a feed-forward capacitor is being used.

    Ben