This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629210: Schematics Review & Power Sequencing of Rails

Part Number: TPS629210
Other Parts Discussed in Thread: TPS62901

Hello,

I've been working on the power supply unit with multiple rails.

The design should have the following output rails: 5V @ 1A, 3.3V @ 1A, 1.8V @ 200mA. I've been using 3x TPS629210 for this task.

Could someone please comment on the schematics, which I am attaching below? I'm mostly curious about sequencing the rails: I would like the 5V Rail to come up first, then 3.3V and 1.8V in the end. Thank you in advance.

Best Regards,

Lukasz Kawinski