Other Parts Discussed in Thread: LM25148, LM5148, LM5146
Hi, I need help in choosing a buck converter IC for the following design requirements. Input = 10 to 60V output = 8.4, 12.4,16.8V respectively(using FB resistors probably) Output current = 10A I also need help in reference design either from Webench or EVM. I checked LM5085 but it's webench do not work for these requirements. EVM also has not similar specs.
Size is very important so i need low BOM count.
I have questions though about EVM design.
Is it advisable to follow the EVM design and change according to the above need? If yes then what particular components i should focus on for the above requirements other than FB resistors.
Thanks