Hi dear people,
at the end, I am going to use the BQ25176J to charge a LIC.
The producer of the LIC recommends the following values:
ISET=750mA
Best charging voltage 3.8V.
If you cannot set 3.8V, please set 3.7V
The data sheet of the BQ25176J lists the resistors for values of:
61.9kΩ for 3.7V or
47.5kΩ for 4.05V
I interpolate a value of 57.8kΩ to obtain 3.8V
Is this ok, or do you have a precise formula to calculate it?
Best regards,
Gustavo