This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HB08-Q1: Request H/W Design Guide

Part Number: TPS1HB08-Q1

I'm trying to use TPS1HB08AQPWPRQ1.

The MAX Current load is 6.8A and the Nominal Current is 4.5A.

The operating range of my controller

is -40℃~+75℃.

I want to cut off the current when the load consumes more than MAX 6.8A current in an environment of -40℃~+75℃.

I checked the range of KCL values.

※ KCL(Current Limit Ratio Version A) = 160 (min:120~max:208 [A*kΩ]

- 1st inquiry: Does this high side switch block the current by cutting it off?
                     Or, I wonder if the maximum current is maintained by limiting the maximum current.

- 2nd inquiry: Because of the range of KCL, I would like to know how much the error value of the blocking current varies depending on temperature.