Other Parts Discussed in Thread: LM5185
Hello guys,
One of my customers is considering using LM25185 for their new products.
They want to build the following spec isolated DCDC with LM25185.
[Spec requirements]
Vin=DC9V~36V(24V typ)
Vo=DC3.3V+/-2%
Io=4A(13.2W)
Small solution size is the highest priority.
Enable control for output on/off.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
Does LM25185 suit to their requirements?
Q2.
Is any special transformer needed?
Q3.
Is there other solution or device to achieve the requirements?
Your reply would be much appreciated.
Best regards,
Kazuya.