Other Parts Discussed in Thread: LM5185,
Good evening at all;
I would like to create a simple PSR Flyback DC/DC Controller for example with the LM5185 features approximately: Vin 30 to 65 Volts and Vout of 30 Volts 3A. Without Auxiliary winding on the T1 transformer.
An architetture similar to the LM5185EVM-SIO schematics.
Obviously by sizing the components and protections much more powerful example; Q1 200 Volt 80A, D2 200 Volt 20 etc...
I also need to replace a much larger and more powerful RF T1 transformer for example the Wurth 749196540 with all the windings in parallel I obtain approximately > 10 A rated and saturation current.
Is it possible that I can obtain similar powers with a simple flyback with the LM5185 controller, or do you recommend other controllers or other configurations that are simple and have few components??
NB: My important degree of freedom of mine; my 30 Volt output voltage does not have to be perfectly regulated and stabilized, it can also have a high ripple, and also vary from 25 V to 35 Volt
Thank you very much