Hi,
We have a PCBA in a product that uses a TPS62177DQCT buck regulator to regulate 25V to 3.3V. Several of the regulators have failed on products and my team has been testing the PCBA to determine the root cause.
We've measured the input voltage and never see it exceed the 28V input rating but there is a part of the device operation that can cause a significant voltage sag on the input to the regulator. We are wondering if this rapid sag could damage the regulator and cause it to fail.
The schematic is below:
Here is an oscilloscope capture of the input voltage transience measured across C37.
Other things we have tested / checked:
-Confirmed the current usage is well below the 500mA rating (we use max 100mA)
-Checked for voltage transience on the input above 28V during different parts of the device operation
-Confirmed the voltage levels on the enable and sleep signals are below their max rated voltages
-Checked the 3v3 output to confirm nothing is leaking onto it to make it too high
-Check the PCBA operating temperature
Thanks for your help