This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5085-Q1: Error in simulation in LTspice

Part Number: LM5085-Q1
Other Parts Discussed in Thread: LM5085

I am trying to simulate a buck converter using the the PSPICE .lib file in LTspice (LM5085_TRANS) and It shows an error that says "Analysis: Time step too small; time= 1.26758e-11, timestep = 1.25e-19: trouble with node "u1:22:1:4"". I get this message even when I try to run the simulation with parts mentioned in the typical application (8.2 of section of datasheet). Can you help me resolving this issue? Also can you suggest what changes should I make to my circuit so that it works.