Hi,
Could you check below and recommend proper component?
Actually customer needs 0.95V but they can accept 1V due to drop by path.
1. Proper feedback resistor for minimum output(1V)
2. Is below inductor proper for the output?
input: 5V, output: 1V and 3.3V, 6A
Inductor: 2.2uH, 9A, 744311220(Wurth Elektronik/Germany)