Other Parts Discussed in Thread: ADS1220, LM2776
Hi TI guys,
Is it reccomended LM2664 in a new project?
i will use it to give negative power supply to ADS1220 AVSS (in order to acquire -0.2V from a sensor) and to deliver negative power supply to an op.amp to erase the offsett.
what about longevity program?
Do you have other part number to suggest to me?
Vin 2,5V to 5V
Vout -0.5V -2.5V
Iout at least 50mA
same case (sot 23) appreciated.
Thanks
Claudio