Other Parts Discussed in Thread: TEST2, LSF0102
Dear TI Engineer,
We used TLV70215DBVR to connect LSF0102DCUR in one of our projects, and the schematic diagram is as follows:
When pulled to 1P5V_GEN on MDC and MDIO, the voltage of 1P5V_GEN will be raised to 2.6V. NET-MDC_1V5 and NET-MDIO1V5 were pulled up to 1P5V_GEN through R371(330 ohms, already removed) and R370(1.5K). However, the actual measurement showed that 1P5V_GEN became 2.6V.
But if the pull-up voltage is changed to DVDD-RG_1.5V output by RTL8111FS PIN29, then the output 1.5V level is normal.
Can you help to analyze the cause of this problem?
Thanks,
Kind Regards