Hi,
I'm currently working on a Dual Active Bridge DC-DC converter project, utilizing the UCC21750 gate driver ICs. The switching frequency of the converter is 20kHz, and we are using SiC MOSFETs as the switching devices. However, we've encountered an issue with two of the gate drivers misbehaving. Specifically, is experiencing a sudden drop in gate voltage to zero, causing the MOSFET to turn off unexpectedly for about 500ns while the input of the gate driver is fine. Strangely, no fault is being triggered from the gate driver IC.
I've reviewed the PCB layout, ensuring that all decoupling capacitors are positioned close to the gate driver ICs with the shortest possible trace length. I've attached a waveform illustrating the issue, notably occurring at a frequency of 1kHz. Could there be any logic within the gate driver that might explain this behavior at 1kHz?
I wanted to provide further details regarding PCB layout. We have used a ground plane in our high-side gate driver, which differs from the PCB design guidelines recommended for the UCC21750. Despite this deviation, I'd like to highlight that I've utilized ground planes in numerous designs previously without encountering any issues.
Any insights or suggestions you may have regarding this issue would be greatly appreciated.