Other Parts Discussed in Thread: TPS27SA08-Q1, TPS1HTC30-Q1,
Hello,
My customer is looking to set a 15-20mA current limit on a 24V rail and they want a HS switch that can be enabled by a 3.3V MCU GPIO pin.
None of our load switches or HS switches that I can see that operate at 24V can set such a low current limit so I was thinking about using a current sense amplifier with an integrated comparator. Issue with this solution is that the comparator output is going to go from low to high when the output current exceeds the threshold and none of our 24V switches have active low enable. Was trying to figure out a way to do this without 3 devices and wanted to check if I was missing something. Lastly, they are hoping for a power good options to indicate if there is an overcurrent condition (I think with the comparator output they could just monitor that).
Thanks!
John