Other Parts Discussed in Thread: UCD9090
A fault happened in our system in which all 4 buck SMPS's turned off, and when we read back some registers after the fault, we see:
INT_TOP: 0xb1
INT_BUCK: 0x03
INT_BUCK_1_2: 0x66
INT_BUCK_3_4: 0x66
INT_VMON: 0x00
INT_GPIO: 0x00
INT_GPIO_1_8: 0x00
INT_STARTUP: 0x00
INT_MISC: 0x01
INT_MODERATE_ERR: 0x08
INT_SEVERE_ERR: 0x00
INT_FSM_ERR: 0x02
Since all 4 bucks show UV/SC happened, what can we get from what happened in this system? Is there any other registers that we can read to get a better picture on what happened? FYI, in our system, when one rail has a fault that leads to it turning off, the system turns all the rails (except the source to LP8764) off.