This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59283: What is the optimal voltage to power 7 segment displays with this part?

Part Number: TLC59283

Hello,

   I'm using a few TLC59283 ICs to drive seven segment displays, HDSP-521G, Vf = 2.0V. For highest efficiency and least heating of the TLC59283, what would be the best voltage to supply the LED displays with? 3.3V or 5.0V? I think I only need about 20mA per segment.

Also, is there a way to use one potentiometer to control the current on threeTLC59283 ICs? Client wants a common brightness control for all the digits.

Thank you,

Derek