Hello,
LM25118-Q1 is used in our design to provide 12V/5A at the output from input 8V~33V. The design is tested many times, the response is good when no load and full load conditions are applied over the entire input range.
UVLU is connected to two resistors to achieve 5V voltage divider network and enable signal is powered from the same input using two diodes oring inputs: 1. manual switch 2. PMOS controlled by MCU signal.
The problem is when input voltage is high (lets say > 26V), the system is working fine with no load and full load conditions. after that, when trying to toggle an external switch to enable the power supply (testing), IC will be damaged, and output voltage drops to 3.7V even at no load condition (the same behavior has been observed for many boards). Also the internal bootstrap diode is shorted.
What is exactly the reason behind this problem and how we can solve it? The problem at the start-up with high input voltage after toggling on the switch. The following image shows the power supply circuit, some components are not populated (DNI) and the input is protected against reverse polarity and overvoltage transients, etc.