This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62095: Maximum spec for high side current limit

Part Number: TLV62095
Other Parts Discussed in Thread: TPS62095, TLV62595, TPS62A06

Hi,

My customer want to check the maximum spec of high side switch current limit, please advise.

Thanks and Best regards,

Tiger

  • Hi,

    Additional question is whether TLV62095 has low side current limit function?
    Because it is not mentioned in the datasheet, suppose it is only with high side current limit feature.

    Thanks and Best regards,

    Tiger

  • Hi Tiger,

    The maximum current limit value is not specified.  The p2p TPS62095 does specify a value.

    This device does not use a low side current limit.

    But these are older devices.  Can you use the TPS62A06 or TLV62595 instead?

    Thanks,

    Chris