Can someone please explain to me what to do with the following information.
If I enter Qe in cell C56 with 0.37, the LLC Gain curve is OK, but in cell C102 it says "CAUTION. Update Cell C57 with new Qe"
If, on the other hand, I enter 0.46 in cell Qe, the LLC gain curve is not ok, but cell C102 says "Gain curve is up to date"
I am a little unsure if I should ignore this information, or if I would be making a mistake in the design if I continue to work with Qe = 0.37.
Many thanks in advance