Hi there
I am using the BQ 24450 to charge a 6V lead acid battery from either a 10.8V OC, 5W solar panel or a 15V power supply. The battery will be connected 24 / 7. My calculations for the circuit at as follows.
Vfloat
6.731466
Volts
Vboost
7.079974
Volts
Vthreshold
5.143104
Volts
When connected to the power supply, the I limit jumper will take the current limit 2.2R path (low charge current). When connected from the solar panel, it will take the 0.33R current limit path.
The three MOSFETs are all P type FDD4243 from fairchild, with plenty of heatsinking for each. http://www.fairchildsemi.com/ds/FD/FDD4243.pdf
My question: what possible failure modes can you think of in the circuit below? (even if unlikely). Your input would be greatly appreciated.....
Thanks