This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG2100R044: Idle power consumption of LMG2100 vs LMG5200.

Part Number: LMG2100R044
Other Parts Discussed in Thread: LMG5200, , LMG2100EVM-078

Hello,

I have been using the LMG5200 for a few years and decided to move to the LMG2100 as it is newer.

I see that with the LMG2100 the idle current draw for the board is 0.12A at 56V.

With the LMG5200 devices, the idle current was 0.08A at 56V.

The power consumption is 2.25W higher with the LMG2100 device.

I would have thought power consumption would be lower as the LMG2100 should be more efficient. Am I looking at this wrong?

Thanks;

Leo