This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Xiaoying
Can you please share what's the customer/EE and the test standard?
Thanks and best regards.
Hi Gui,
It is air conditioner application.
They are doing ESD test: 15kV ESD (air), but tps54202 will fail this test.
Customer wants to find a device with higher ESD rating, can you help confirm?
BR,
Xiaoying
Hi Xiaoying
Please let me check about this and get back to you later.
Than you!
Hi xiaoying
Did customer do the ESD test on the TPS54202 or on their system board? On what pin did they perform the ESD test?
Thank you!
Hi Gui,
I just want to quick check that from datasheet spec perspective, if we have higher ESD rating device.
I can also check all the available datasheet but it will be very slow.
BR,
Xiaoying
Hi Xiaoying
I will check about this. Is >20V, 2A device needed?
Thank you!
Hi Xiaoying
For MVB devices, I’m not aware any other device with higher ESD Spec on Datasheet.
Thanks and best regards.