Other Parts Discussed in Thread: BQ25672, , , TUSB320, TPS25751, TPS25751EVM, , TPS26750, TPS2663
Hi, This is Dan Fasano. You have answered many questions I had on the BQ25672 a few months ago, so thank you for that.
I did an entire design based upon the BQ25672 and it was reviewed by TI. Now we are thinking the BQ25756 (maybe the E version?) is
a better choice.
The higher input voltage for the BQ25756 allows us to only have 1 power input, that is the primary motivation.
We have to operate in an aircraft environment with a 28V primary power source or USB-C at 20V.
Also, we need to support only a single cell Li battery.
If you can point out any other differences between the BQ25672 and the BQ25756 that would be great.
Thanks,
Dan