Other Parts Discussed in Thread: TPS552872
Hey Buck Regulator Team,
I have a customer considering using the LMR23625 for a new project and we were hoping you could provide some feedback and design guidance.
The key requirements are outlined below:
1. Cost target: $1
2. Foot print: ~210 mm^2
3. 3.5V minimum, 12V nominal. 30V max
4. Current rating of 2A.
5. Adjustable output Voltage. The nominal voltage is 5.15V
6. Output Sink current capable
The device would need to be used in a topology that allows for a positive output voltage that can be greater than, equal to or less than VIN. They are currently considering LMR23625 due to this post about using this regulator in a Zeta topology: LMR23625 or LMR23630: Zeta Converter Buck/Boost implementation
Do you recommend this solution or should we be considering a different option?
-Matt Calvo