Other Parts Discussed in Thread: UCC28056, PMP40580, UCC25660, UCC28782, UCC256301
I starting to design a DC/DC converter that will take a 450VDC rail and put out an isolated voltage from between 80V and 285V, with a regulated constant current. The current will be user-programmable, up to 900mA, but with an output power not exceeding 180W (so at an output voltage of 285V, the max current would be limited to 630mA). I am having a little trouble finding reference designs or decent analysis of a topology that will work across such a large output voltage range. I came across the PMP40580 demo board, which uses the UCC28056 and UCC256404 chips, which I'm looking into using as a starting point, but wanted to see if there was another chipset that'd be better suited for this application. I'm not so concerned with the PFC stage - that's a pretty straight-forward design.
Thanks,
Joe