Hi,
I wanted to change the OVP of U2 on LM73100EVM but did not get the result, please help to see what i had missed out for the below 6 steps?
1) Tested the default settings on EVM and is working for OVP=13.76V using R17=191K.
2) Using the Overvoltage Formula below with R14=2M, i calculated R17=113K for OVP=22V (Vov).
Vov=1.2*[(2M+113K)/113K]
3) I replaced R17 from 191K to 113K on the EVM.
4) Connected Power Supply input to EVM and slowly increased 1V per step beginning from 3V.
5) When the Power Supply voltage level passes the default UV=10.84V setting, i can see LM73100 start to conduct power.
6) When the Power Supply voltage increased to 15V, i noticed the Power Supply voltage dropped to zero and maximum current was drawn (looks like short circuit).
Whereas I was expecting LM73100 continue to conduct power until the Power Supply voltage input reached 22V.
Thank you,