Other Parts Discussed in Thread: TPS650002-Q1
Hi, I am looking for a PMIC to power the OX01F10 image sensor, could you help me to select a type of PMIC to meet following requirements:
Output of PMIC:
Rail 1: 3.3V(AVDD) Rail: Up to 300 mA
Rail 2: 1.8V(DVDD): Up to 600 mA
Rail 3: 1.1V(DOVDD): Up to 600 mA
Sequence: can rise in any order
Input of PMIC:
PVIN for PMIC is 3.3V.
TPS650320-Q1 has 4V as min voltage, but our max input voltage is only 3.3V , we have to choose another one.
thanks
Frank