Hi Team,
I need to verify the Load and Line transient response of the part REG104 3.3V.
In datasheet, they given spec as below
as I have seen, the load transient has spec of around 500mV overshoot and 650mV undershoot for 0uF cap, and 200mV overshoot and 300mV undershoot for 10uF cap, but I got the result for 0uF but getting same result for 10uF also, even If I increase the cap to 20uF also, getting same response as 0uF.
Also, for Line transient response, I'm not getting the spec for both 0 and 10uF cap, kindly help to resolve as I need to verify transient to make sure it will not impact on future.