Other Parts Discussed in Thread: BQ25886, BQ25798
Hello Sir,
can we charge with input of 5v and the is battery of 8.4V Lipo.
if we want to charge with 5V VUSB charger with 1pack (4.2V Lipo) and 2 pack (8.4V Lipo)Cell?
and also, problems which i am facing my output voltage at VBAT is 2.87V only its showing i trying with the Voltage divider with 562K for the 4.2V at out and another case is 1.33M RESISTORs for 8.4V at output charge but my output is showing 2.87V and the if i give the EN pin HIGH the system is getting to drop out at output.