This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56837H:TPS56837H works for a short time and stops.

Part Number: TPS56837H

Good afternoon, I made a circuit using the CI texas TPS56837H for testing and evaluation, but I couldn't get the IC to work properly as expected. when feeding the IC with a low voltage (6 to 10 V) the output is activated and regulated, but with a higher voltage it stops working and burns, does not short circuit, but ends up stopping and no longer returning to "life".  I put a potentiometer in the circuit to be able to adjust the output voltage but I don't know if this is possible with the circuit in operation.   I need help as I have already damaged 3 CI's. I'll leave the schematic of the circuit. Thanks in advance for the help and I'm sorry for my English which is not very good.