Hi,
Is it possible to trick the TPS61196 that the LED strings are connected, when they in fact are open circuit? For example if I would apply a voltage (higher than the IFBV and lower than the V_LED_SHORT) to the IFB pins at the same time as I disconnect (open) the LED strings?
If possible, would I also have to do something with output voltage to keep it steady when LED strings are open to prevent OVP to kick in?
Kind regards, Simon