Other Parts Discussed in Thread: TPS25984, LM5148
Tool/software:
Hello,
I am working on a DC/DC buck converter for automotive application using LM5148-Q1 buck controller. Since the application has high safety/reliability requirements, we are thinking of adding an eFuse at the output of the DC/DC. In particular, the TPS25984. Here are some context of our design:
- Load current: 10A continuous (80% life), 25A max (20% life)
- Larger risk: short-circuit on the load side
- eFuse functionality: no need for telemetry or COM, operating as single stand-alone design
I am not very familiar with the inner working mechanism of eFuses, so I wonder if the addition of TPS25984 to the buck output would actually justify its added cost. The main reason is that the LM5148-Q1 already has a suite of built-in protections. The advantages of adding TPS25984 that I currently see is:
- Faster short-circuit protection (the eFuse will provide more rapid response to catastrophic short)
- Handling buck output capacitor current surge (since the eFuse will be downstream from the output capacitor, it will be able to limit current provided by the capacitor even when the inductor current is already limited by the LM5148)
- Redundancy (having two protection circuitry with autoreset provide added safety/reliabity when either fails)
That said, we are not really utilizing much of the telemetry, COM, or thermal sensing provided by the eFuse. We really just need the eFuse to act like a mechanical fuse that is resettable. Thus, even though there are benefits, it is not immediately clear to me whether they are significant.
I would really appreciate your opinons and experience on this,
Thank you!