Tool/software:
Hello experts,
I am working on TPS6594-Q1 PMIC device,
I put a break point after writing the answers in long window, the device resets.
If I break point after writing the answers in window1, the device resets. and same for the window2.
I see the correct answers are written for the respective question generation.
Even without any breakpoints also, there is a resetting of the device after the window2.There is no possibility of going for next question generation.
I read the value of the WD_FAIL_CNT as 0x0.
I have configured enough time for the long window also (WD_LONGWIN is configured to the value of 0xFF). Window 1 and window 2 are configured for their max values.
What else can be the reason for the reset behavior of the device
Thanks in advance
Kind Regards
Manisha Narayan Gowda