This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987DDK: Detailed information on TPS65987 GPIO

Part Number: TPS65987DDK
Other Parts Discussed in Thread: TPS65987DJEVM, TPS65987, TPS6598X-CONFIG, TUSB320

Tool/software:

Dear Sirs and Madams,

We are considering TPS65987DDK based on TPS65987DJEVM.

We would like to know the following two points about the GPIO of the TPS65987.

 

1.

In the TPS65987DDK datasheet, Although an explanation of the dedicated terminal is provided for some GPIOs, detailed explanations are not provided for many GPIOs.

I understand that you can assign functions to GPIOs using TPS6598X-CONFIG, but can you freely assign functions to all GPIOs?

Is there any documentation that describes the functions that can be realized with the GPIO of the TPS65987?

2.

We would like to incorporate an ID pin function for USB OTG into the TPS65987, like the TUSB320.

Is it possible to incorporate this functionality into the GPIO of TPS65987 using TPS6598X-CONFIG?

Regards,

MM