Tool/software:
From one day to the next, the voltage regulator I was using developed a low impedance (16ohms) between pins 4 and 5 on the WSON package. As EN was also tied to the Vin, this caused the supply for the circuit to go into current compliance (gratefully) and fail to provide a high enough voltage for the regulator to provide 5V. With the regulator removed from the board, the impedance between the two pins still measures 16 ohms. Is this a known failure mode for this component?