This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: 06

Part Number: BQ77915

Tool/software:

Hi,

I have designed BMS with Internal Cell Balancing using BQ7791506. But Cell Balancing not working .Please see the  test results below:

4 Cells are in Series. 5AH Battery

Before Charger Connected - Cell Voltages 

Cell - 1  -- 3.34V

Cell - 2  -- 3.34V

Cell - 3  -- 3.34V

Cell - 4  -- 3.30V

After Charger Connected - Cell Voltages (Time: 10.08AM IST)

Cell - 1  -- 3.47V

Cell - 2  -- 3.47V

Cell - 3  -- 3.46V

Cell - 4  -- 3.39V

Cell Voltages (Time: 10.13AM IST)

Cell - 1  -- 3.52V

Cell - 2  -- 3.53V

Cell - 3  -- 3.51V

Cell - 4  -- 3.38V

Cell Voltages (Time: 10.27AM IST)

Cell - 1  -- 3.66V

Cell - 2  -- 3.62V

Cell - 3  -- 3.51V

Cell - 4  -- 3.34V

Here 4th Cell is at down side and that cell is started discharging but other cells are charging more than 3.5V. But as per datasheet for BQ7791506 cell balancing start at 3.5V. No cell balancing observed  Please explain the what's the problem and why Cell 4 is only discharging more. I have used Rin resistor 33E and Cin 1uF