Tool/software:
Please tell me the maximum rated power consumption for the above model name.
The value at 25℃ is fine.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Please tell me the maximum rated power consumption for the above model name.
The value at 25℃ is fine.
Hello,
The power consumption will depend on the output power of the device. The device has a maximum output current of 3A. The input current will depend on your duty cycle. For quiescent current, please refer to Section 7.10 of the datasheet.
Best regards,
Ridge
It is true that "power consumption" depends on the output power, but what we want to confirm here is:
Since I have confirmed the "absolute maximum rated power", please tell me the maximum allowable power at 25℃.
There should be a similar description for normal devices.