Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hello. I'm having trouble connecting the TPS65235EVM-694 module to the SLVC651 GUI through either the USB2ANY module and the USB-to-GPIO module.
I followed the instructions on the manual for the EVM kit and it doesn't seem to connect to the board, the registers cannot write or read anything.
I've set up the board, from what I researched, appropriately for software connection but I haven't been able to successfully get a connection.
The other issue I was having too, before I tried to connect to the software for this EVM kit was while setting up the voltage output manually to be 13.4V with a tone imposed on it, I double checked the tone to see if it was an accurate 22kHz tone. With no load the tone resembles a sawtooth wave and does not look correct, only if an external circuit is applied or some kind of load, roughly 200mA, will it actually look correct.
If anyone could offer some advice for these issues I'd greatly appreciate it!