Part Number: UCC28056
Tool/software:
Hello,
I am designing a PFC using the UCC28056A IC. I have an issue where the PFC does not regulate to the set voltage. For example, when I set the output voltage to 300V, the output reaches this voltage and works normally. But when I start increasing the output voltage setpoint towards 500V at some point it just stops increasing the voltage and stays at 425V. I have noticed that when I try increasing the output voltage setpoint above this voltage, the VOSNS voltage starts dropping from 2.5V to 2.0V.
Here is a capture of the VOSNS, ZCD and fet drain voltages:
The blue signal is VOSNS and it is steady around 2.0V

I have also measured the ZCD signal closely to see if there is an overcurrent protection OCP1 happening, but the ZCD signal during on-interval does not exceed 500mV to trip OCP1. It only reaches ~50mV. Here is a capture of ZCD and drain voltage:

After this I also measured the COMP voltage. Unfortunatelly I don't know how to interpret this signal and I ask you for help and advice on what should the signal look like.

To make things worse, when i increase the input AC voltage, the PFC starts pulsating. I deduced that OCP2 is triggering since the interval between separate pulses is 1s, as is the delay when OCP2 is triggered. Here is a capture of this pulsation.

I dont understand why OCP2 is triggering since the ZCD/CS signal during on-time reaches only 60mV which is far from 750mV threshold to trigger OCP2.
I am attaching the Altium project so you can see the schematics and PCB layout. I am also attaching the UCC28056 excel calculator I used to design the circuit.
I thank you for your help.
Samo
240613 UV Bulb Driver Altium - TI e2e ticket.zip
260613 UCC28056X_Design Calculator v02 120Vac TI e2e ticket.xlsm