This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Bq34z100g1

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ34Z100, BQ34Z100EVM

Tool/software:

I am using bq34z100g ics in my two identical boards.

I connected the boards to PC via EV2400 and found ....

1. Device address of one Ic: 10h and other board ic is AA h

2. One board golden image and reading the content through bqstudio software failed and other is board is following all instructions perfectly 

3. Sealing , unsealing access from Bqstudio software to bq34z100 is not working whereas for other board, this application are working 

Is the ics are fine or any other issues which can be addressed 

Regards

Saptarishi